7.4.4 Near Objects
The __near qualifier can be used to indicate that variables or functions
are located in ‘near memory’. Exactly what constitutes near memory is dependent on the
target device, but it is typically memory that can be accessed with less complex code.
Expressions involving near-qualified objects generally are faster and result in smaller
code.
Use the native keywords discussed in the Differences section to look up information on the semantics of this qualifier.
Some devices may not have such memory implemented, in which case, use of this qualifier
is ignored. Stack-based (auto and parameter) variables cannot use the
__near specifier.
Example
The following shows a variable and function qualified using __near.
__near int serialNo;
__near int ext_getCond(int selector);
Differences
When targeting PIC devices, the MPLAB XC8 compiler has allowed the near
specifier to be used with variables. This specifier has not been allowed with functions.
When targeting AVR devices, MPLAB XC8 has not implemented any “near” memory.
The MPLAB XC16 and XC-DSC compilers have used the near attribute with
both variables and functions.
The MPLAB XC32 compiler has used the near attribute for functions,
only.
Migration to the CCI
When targeting PIC devices with the MPLAB XC8 compiler, change any occurrence of the
near qualifier to __near, for example, from:
near char template[20];
to:
__near char template[20];
When using the other compilers, change any occurrence of the near
attribute to the __near specifier, for example, from:
void bar(void) __attribute__ ((near));
int tblIdx __attribute__ ((near));
to
void __near bar(void);
int __near tblIdx;
Caveats
None.