4.3.6 Pointer Types
There are two basic pointer types supported by the MPLAB XC8 C Compiler:
- Data pointers
- These hold the addresses of objects which can be read (and possibly written) by the program.
- Function pointers
- These hold the address of an executable function which can be called via the pointer.
These pointer types cannot be used interchangeably. Data pointers (even
generic void * pointers) should never be used to hold the address of
functions and function pointers should never be used to hold the address of objects.