| “The number of bits in a byte (C90 3.4, C99
3.6).” |
| 8. |
| “The values of the members of the execution
character set (C90 and C99 5.2.1).” |
| The execution character set is ASCII. |
| “The unique value of the member of the execution
character set produced for each of the standard alphabetic escape sequences
(C90 and C99 5.2.2).” |
| The execution character set is ASCII. |
“The value of a char object into
which has been stored any character other than a member of the basic execution
character set (C90 6.1.2.5, C99 6.2.5).” |
| The value of the char object is the 8-bit binary
representation of the character in the source character set. That is, no
translation is done. |
“Which of signed char or
unsigned char has the same range, representation, and behavior as
“plain” char (C90 6.1.2.5, C90 6.2.1.1, C99 6.2.5, C99
6.3.1.1).” |
| By default, signed char is functionally equivalent to
plain char. If the CCI is specified, then the default is
unsigned char The options -funsigned-char
and -fsigned-char can be used to explicitly specify the
type. |
| “The mapping of members of the source character
set (in character constants and string literals) to members of the execution
character set (C90 6.1.3.4, C99 6.4.4.4, C90 and C99 5.1.1.2).” |
| The binary representation of the source character set is preserved to the
execution character set. |
| “The value of an integer character constant
containing more than one character or containing a character or escape sequence
that does not map to a single-byte execution character (C90 6.1.3.4, C99
6.4.4.4).” |
| The previous value is shifted left by eight, and the bit pattern of the
next character is masked in. The final result is of type int.
If the result is larger than can be represented by an int, a
warning diagnostic is issued and the value truncated to int
size. |
| “The value of a wide character constant containing
more than one multibyte character, or containing a multibyte character or
escape sequence not represented in the extended execution character set (C90
6.1.3.4, C99 6.4.4.4).” |
| Multi-byte characters are not supported in source files. |
| “The current locale used to convert a wide
character constant consisting of a single multibyte character that maps to a
member of the extended execution character set into a corresponding wide
character code (C90 6.1.3.4, C99 6.4.4.4).” |
| Multi-byte characters are not supported in source files. |
| “The current locale used to convert a wide string
literal into corresponding wide character codes (C90 6.1.4, C99
6.4.5).” |
| Wide strings are not supported. |
| “The value of a string literal containing a
multibyte character or escape sequence not represented in the execution
character set (C90 6.1.4, C99 6.4.5).” |
| Multi-byte characters are not supported in source files. |