| “The mapping between physical source file
multibyte characters and the source character set in translation phase 1
(5.1.1.2).” |
| “The name and type of the function called at
program start-up in a freestanding environment (5.1.2.1).” |
| int main (void); |
| “The effect of program termination in a
freestanding environment (5.1.2.1).” |
| Interrupts are disabled and the programs loops indefinitely |
“An alternative manner in which the
main function may be defined (5.1.2.2.1).” |
| void main (void); |
“The values given to the strings pointed to by the
argv argument to main (5.1.2.2.1).” |
| No arguments are passed to main. Reference to
argc or argv is undefined. |
| “What constitutes an interactive device
(5.1.2.3).” |
| Application defined. |
| “The set of signals, their semantics, and their
default handling (7.14).” |
| Signals are not implemented. |
“Signal values other than SIGFPE,
SIGILL, and SIGSEGV that correspond to a
computational exception (7.14.1.1).” |
| Signals are not implemented. |
“Signals for which the equivalent of
signal(sig, SIG_IGN); is executed at program start-up
(7.14.1.1).” |
| Signals are not implemented. |
“The set of environment names and the method for
altering the environment list used by the getenv function
(7.20.4.5).” |
| The host environment is application defined. |
“The manner of execution of the string by the
system function (7.20.4.6).” |
| The host environment is application defined. |