3.6.2.9 Help
The --help option displays information on the
compiler options, then the driver will terminate.xc8-cc
The displayed help might differ for
different device families, which can be indicated using the -mcpu option.
Note that options displayed by the --help command that are not documented in
this compiler user's guide might not be supported. See the MPLAB®
XC Compiler Functional Safety Manual for options approved for use in functional
safety applications.
For
example:
xc8-cc -mcpu=atmega48pb --help
Usage: avr-gcc [options] file...
Options:
-pass-exit-codes Exit with highest error code from a phase
--help Display this information
--target-help Display target specific command line options
--help={common|optimizers|params|target|warnings|[^]{joined|separate|undocumented}}[,...]
Display specific types of command line options
(Use '-v --help' to display command line options of sub-processes)
--version Display compiler version information
-dumpspecs Display all of the built in spec strings
-dumpversion Display the version of the compiler
-dumpmachine Display the compiler's target processor
-print-search-dirs Display the directories in the compiler's search path
-print-libgcc-file-name Display the name of the compiler's companion library
-print-file-name=<lib> Display the full path to library <lib>
-print-prog-name=<prog> Display the full path to compiler component <prog>
-print-multiarch Display the target's normalized GNU triplet, used as
a component in the library path