13.2 Type References
Another way to refer to the type of an expression is with the
            typeof keyword. This is a non-standard extension to the language. Using
         this feature reduces your code portability.
The syntax for using this keyword looks like sizeof, but
         the construct acts semantically like a type name defined with typedef.
There are two ways of writing the argument to typeof:
         with an expression or with a type. Here is an example with an expression:
typeof (x[0](1))
This assumes that x is an array of functions; the type
         described is that of the values of the functions.
Here is an example with a typename as the argument:
typeof (int *)
Here the type described is a pointer to int.
If you are writing a header file that must work when included in ANSI C
         programs, write _ _typeof_ _ instead of typeof.
A typeof construct can be used anywhere a
            typedef name could be used. For example, you can use it in a
         declaration, in a cast, or inside of sizeof or
         typeof.
- This declares 
ywith the type of whatxpoints to:typeof (*x) y; - This declares 
yas an array of such values:typeof (*x) y[4]; - This declares 
yas an array of pointers to characters:typeof (typeof (char *)[4]) y;It is equivalent to the following traditional C declaration:
char *y[4]; 
To see the meaning of the declaration using typeof, and
         why it might be a useful way to write, let’s rewrite it with these macros:
#define pointer(T) typeof(T *)
#define array(T, N) typeof(T [N])
Now the declaration can be rewritten this way:
array (pointer (char), 4) y;
Thus, array (pointer (char), 4) is the type of arrays of
         four pointers to char.