25 C++ Implementation-Defined Behavior
The ISO C++ standard requires a conforming implementation to document the choices for behaviors defined in the standard as “implementation-defined.” The following table lists all such areas, the choices made for the compiler, and the corresponding section number from the ISO/IEC 14882:2014 C++ Standard.
| ISO Standard | Implementation | 
|---|---|
| Which of the compiler's output messages are diagnostic messages (1.3.6) | |
All output to stderr is a diagnostic. | |
| The required libraries for a freestanding implementation (1.4) | |
| See the response for The set of headers for a freestanding implementation (17.6.1.3). | |
| The number of bits in a byte (1.7) | |
| 8 bits | |
| What constitutes an interactive device (1.9) | |
If isatty() is true, then interactive stream support
                            is implied. | |
| The number of threads in a program under a freestanding implementation (1.10) | |
| Threads are not directly supported. | |
| How physical source file characters are mapped to the basic source character set (2.2) | |
| The locale settings determine the default source character set or UTF-8 if this cannot be determined by the locale. The basic source character set is UTF-8. | |
| Physical source file characters (2.2) | |
Defaults to the set locale and if that doesn’t work, defaults to
                            UTF-8. Can be any encoding supported by the system’s
                                iconv() library routine. | |
| The execution character member chosen for a source character that does not map to an equivalent execution character. (2.2) | |
| ABI Defined | |
| Whether source of translation units must be available to locate template definitions (2.2) | |
| The source must be available. | |
| The execution character-set and execution wide-character set (2.3) | |
The execution character set contains
                                [a-zA-Z0-9_{}[]#()<>%:;.?*+-/^&|∼!=,\"’],
                            space, control characters representing horizontal tab, vertical tab,
                            form feed, new-line, alert, backspace, carriage return, and a null
                            character. The execution wide-character set is the same, except instead
                            of a null character it has a null wide character. Encoding can be
                            anything supported by the system’s iconv() library
                            routine, defaulting to UTF-8 (or UTF-32, for the wide-character
                            set). | |
| The mapping header name to header or external source file (2.9) | |
| Same name as the header, in UTF-8. | |
| The encoding of universal character name not in the execution character set (2.14.3) | |
\UNNNNNNNN or
                                    \uNNNN, where
                                    N is a hex-quad, corresponding
                            to the character short name in ISO/IEC 10646
                                    NNNNNNNN or
                                    0000NNNN,
                            respectively. | |
| The semantics of non-standard escape sequences (2.14.3) | |
As an extension, GCC supports the sequence '\e' to
                            act as the ASCII ESC character. | |
| The value of a character literal outside the range of the corresponding type (2.14.3) | |
| The last byte of the series of bytes making up the literal. | |
| The wide-character literal with single c-char that is not in execution wide-character set (2.14.3) | |
| The last four bytes of the series of bytes making up the literal. | |
| The choice of a larger or smaller value of floating literal when the value is not in the range of representable values for its type (2.14.4) | |
| As per Annex F of C99. | |
| The concatenation of string literals other than those fully specified by the standard (2.14.5) | |
| No extra concatenations are supported. | |
| Whether all string literals are distinct (that is, are stored in non-overlapping objects) (2.14.5) | |
| String literals are not necessarily distinct. | |
The linkage of main()
                            (3.6.1) | |
| External linkage. | |
| The parameters to main (3.6.1) | |
or
                             | |
| What constitutes start-up and termination in freestanding environment (3.6.1) | |
Determined by the device-specific startup code. The default code
                            shipped in a DFP calls constructors before main() for
                            objects of namespace scope with static storage duration but does not
                            call destructors after return from main(). | |
| Whether defining main is required in a freestanding environment (3.6.1) | |
Yes - The device-specific startup code can be customized to not call
                                main(), but some features such as the stack-usage
                            report require main(). | |
| Whether dynamic initialization of a non-local variable with static or thread storage duration is done before the first statement of the initial function of the thread (3.6.2) | |
| Threads are not directly supported. | |
Whether dynamic initialization of a
                            non-local variable with static storage duration is done before the first
                            statement of main() (3.6.2) | |
| Determined by the device-specific startup code, but the default startup code provided in a DFP does call the constructors. | |
| Whether an implementation has relaxed or strict pointer safety (3.7.4.3) | |
| Relaxed pointer safety. | |
| The extended signed integer types (3.9.1) | |
| None | |
The representation of char
                            (3.9.1) | |
| One byte. | |
The signedness of a plain
                                char (3.9.1) | |
A plain char is unsigned. | |
| The value representation of floating-point types (3.9.1) | |
| IEEE-754 | |
| The value representation of pointer types (3.9.2) | |
| 32 bits. | |
| The number of bytes between successive addresses at which a given object can be allocated alignment (3.11) | |
| Valid alignments are powers of 2 up to and including 228. | |
| Whether any extended object alignments are supported and the contexts in which they are supported (3.11) | |
| Extended alignments up to 228 are allowed, subject to the device memory layout. | |
| The value of the result of unsigned to signed conversion (4.7) | |
| For conversion to a type of width N, the value is reduced modulo 2N to be within range of the type. | |
| The result of an inexact floating-point conversion (4.8) | |
| Software emulation uses Round to Nearest but the mode can be changed when using a hardware FPU. | |
| The value of result of inexact integer to floating-point conversions (4.9) | |
| As per C99 Annex F. | |
| The rank of extended signed integer type (4.13) | |
| Extended signed integer types are not supported. | |
| Passing an argument of class type through ellipsis (5.2.2) | |
| Supported | |
The class publicly derived from
                                std::type_info which can be returned by
                                typeid (5.2.8) | |
No extra class is defined. The result is
                                std::type_info. | |
| The conversions between pointers and integers (5.2.10) | |
| A cast from an integer to a pointer or vice versa uses the binary
                            representation of the source type, reinterpreted as appropriate for the
                            destination type. If the source type is larger than the destination type, the Most Significant bits are discarded. When casting from a pointer to an integer, if the source type is smaller than the destination type, the result is sign extended. When casting from an integer to a pointer, if the source type is smaller than the destination type, the result is extended based on the signedness of the source type.  | |
| The meaning of converting a function pointer to an object pointer type or vice versa (5.2.10) | |
| Conversion is supported. The binary representation is preserved. | |
The result of sizeof when
                            applied to fundamental types other than char,
                                signed char, and unsigned char
                            (5.3.3) | |
See Integer Data Types, noting that sizeof() returns a
                            size in bytes. | |
| Whether over-aligned types are supported (5.3.4, 20.7.9.1, 20.7.11) | |
| Yes. | |
The type of ptrdiff_t (5.7,
                            18.2) | |
int | |
| The result of a right shift of negative values (5.8) | |
| Bitwise operators act on the representation of the value including both the sign and value bits, where the sign bit is considered immediately above the highest-value value bit. | |
The meaning of attribute
                            declaration (7) | |
| See Variable Attributes and Function Attributes. | |
| The underlying type for enumeration (7.2) | |
If the enumeration values are all non-negative, the type is
                                unsigned int, else it is int.
                         | |
The meaning of the asm
                            declaration (7.4) | |
| See Using Inline Assembly Language. | |
| The semantics of linkage specifiers (7.5) | |
| Only “C” and “C++” linkage are supported. | |
| The behavior of non-standard attributes (7.6.1) | |
| See Variable Attributes and Function Attributes. | |
| The behavior of an attribute-scoped-token (7.6.1) | |
Attributes are available in the “gnu” namespace and are equivalent to
                                __attribute__. | |
The string resulting from
                                __func__ (8.4.1) | |
| Treated as a constant expression and can be used in constexpr contexts. The string contains the function name only. | |
| The allocation of bit-fields within a class object (9.6) | |
| Bit fields are allocated left to right. | |
| The alignment of bit-fields within a class object (9.6) | |
| Each member is located to the lowest available offset allowable according to the alignment restrictions of the member type. | |
| The semantics of linkage specification on templates (14) | |
Only "C" and "C++" linkage are
                            supported. | |
Whether the stack is unwound before a call
                            to std::terminate() (15.3, 15.5.1) | |
| The stack is not unwound. | |
Whether the stack is unwound before calling
                                std::terminate() when a noexcept
                            specification is violated (15.5.1) | |
| The stack is not unwound. | |
The numeric values of character literals in
                                #if directives (16.1) | |
| Interpreted in the same manner as they would on the target. | |
| Whether a single-character character literal may have a negative value (16.1) | |
| No | |
| The manner of search for included source files (16.2) | |
| Sequential, through a defined list of search paths. The search ends on the first match. | |
The nesting limit for
                                #include directives (16.2) | |
| XC32 imposes a limit of 200 levels to avoid runaway recursion. | |
The search locations for headers included
                            using "" (16.2) | |
The #include "file" directive is
                            used for header files defined by your project. XC32 searches for the
                            file in the directory containing the current source file, then in the
                            quote directories, and then in the system directories. You can prepend
                            directories using a command-line option. | |
The search locations for headers included
                            using <> (16.2) | |
The #include <file> directive
                            is used for system header files packaged with XC32. You can prepend
                            search directories using a command-line option. Directories are searched
                            in the following
                            order: | |
| The sequence of places searched for a header (16.2) | |
| Quote form includes search the directory of the current file, then in the system directories. Angle-bracket form includes only search the system directories. | |
The behavior of a #pragma
                            directive (16.6) | |
| See Pragma Directives. | |
The text equated to
                                __DATE__ when date of translation is not available
                            (16.8) | |
Expands to "??? ?? ????" | |
The text equated to
                                __TIME__ when time of translation is not available
                            (16.8) | |
Expands to "??? ?? ????" | |
Whether __STDC_VERSION__ is
                            a predefined macro and what it means (16.8) | |
This macro is a long integer constant that has the format
                                    yyyymmL, where
                                    yyyy is the year and
                                    mm is the month of the C
                            Standard version with which the compiler is compatible. This shows the C
                            Standard version to which the compiler conforms. | |
Whether __STDC__ is a
                            predefined macro and what it means (16.8) | |
| In normal operation, this macro expands to the constant 1, to signify that this compiler conforms to ISO Standard C. | |
| The set of headers for a freestanding implementation (17.6.1.3) | |
Every header required by the standard except
                                <atomic>, those
                            being: | |
Whether a name from the C standard library
                            declared with external linkage has extern "C"
                                or extern "C++" linkage (17.6.2.3) | |
extern "C++" | |
| The exceptions thrown by standard library functions that do not have an exception specification (17.6.5.12) | |
| There are no implementation-defined exception classes. | |
The error_category for
                            errors originating outside the operating system (17.6.5.14) | |
| None. | |
The type of size_t
                            (18.2) | |
unsigned int | |
| The form of the exit status returned to the host environment (18.5) | |
| Host environments are not supported. | |
The return value of
                                bad_alloc::what (18.6.2.1) | |
| The name of the class. | |
The return value of
                                type_info::name() (18.7.1) | |
| The mangled type name. | |
The return value of
                                bad_cast::what (18.7.2) | |
| The name of the class. | |
The return value of
                                bad_typeid::what (18.7.3) | |
| The name of the class. | |
The result of
                                exception::what (18.8.1) | |
| The name of the class. | |
The return value of
                                bad_exception::what (18.8.2) | |
| The name of the class. | |
| The use of a non-POF (non-“plain old function”) as signal handler (18.10) | |
| Signals are not supported. | |
The exception type when the
                                shared_ptr constructor fails (20.8.2.2.1) | |
std::bad_alloc  | |
Whether placeholder types are
                                CopyAssignable (20.9.9.1.4) | |
| Yes. | |
| Whether extended alignment is supported (20.10.7.6) | |
| Yes. | |
Whether values are rounded or truncated to
                            the required precision when converting between time_t
                            values and time_point objects (20.12.7.1) | |
| Values are truncated. | |
The type of streamoff
                            (21.2.3.1) | |
long long | |
The type of streampos
                            (21.2.3.1) | |
Synonym for
                             | |
The return value of
                                char_traits<char16_t>::eof (21.2.3.2) | |
int_type(-1) | |
The type of u16streampos
                            (21.2.3.2) | |
Synonym for fpos<mbstate_t> | |
The return value of
                                char_traits<char32_t>::eof (21.2.3.3) | |
int_type(-1) | |
The type of u32streampos
                            (21.2.3.3) | |
Synonym for fpos<mbstate_t> | |
The type of wstreampos
                            (21.2.3.4) | |
Synonym for fpos<mbstate_t> | |
| Whether locale object is global or per-thread (22.3.1) | |
| Locale object is global. | |
The effect on C locale of calling
                                locale::global (22.3.1.5) | |
If the locale has a name, same as
                            setlocale(). | |
The value of
                                ctype<char>::table_size (22.4.1.3) | |
SCHAR_MAX + 1 | |
The additional formats accepted for
                                time_get::do_get_date (22.4.5.1.2) | |
| None | |
Whether
                                time_get::do_get_year accepts two-digit year
                            numbers (22.4.5.1.2) | |
| Two-digit year numbers are accepted. | |
The formatted character sequence generated
                            by time_put::do_put in the C locale
                            (22.4.5.3.2) | |
Same as strftime() | |
The type of
                                array::const_iterator (23.3.2.1) | |
const T* | |
The type of array::iterator
                            (23.3.2.1) | |
T* | |
The default number of buckets in
                                unordered_map when this is not specified with the
                            constructor (23.5.4.2) | |
| 0 | |
The default number of buckets in
                                unordered_multimap when this is not specified with
                            the constructor (23.5.5.2) | |
| 0 | |
The default number of buckets in
                                unordered_set when this is not specified with the
                            constructor (23.5.6.2) | |
| 0 | |
The default number of buckets in
                                unordered_multiset when this is not specified with
                            the constructor (23.5.7.2) | |
| 0 | |
The underlying source of random numbers for
                                random_shuffle (25.3.12) | |
It uses rand() as the source of randomness. | |
The effect of calling
                                ios_base::sync_with_stdio after any input or output
                            operation on standard streams (27.5.3.4) | |
| The synchronization referred to is only that between the standard C facilities and the standard C++ objects. User-declared streams are unaffected. | |
The argument values used to construct the
                                fail object of basic_ios::failure
                            thrown by basic_ios flags functions (27.5.5.4) | |
const char& | |
Whether sequence pointers are copied by
                                basic_stringbuf move constructor (27.8.2.1) | |
| Sequence pointers are copied. | |
The effect of calling
                                basic_streambuf::setbuf with non-zero arguments
                            (27.8.2.4) | |
| If no buffer has already been created, and both arguments are non-zero, then the first argument is used as a buffer. | |
Whether sequence pointers are copied by
                                basic_filebuf move constructor (27.9.1.2) | |
| Sequence pointers are copied. | |
The effect of calling
                                basic_filebuf::setbuf with non-zero arguments
                            (27.9.1.5) | |
| The first argument is used as a buffer. | |
The effect of calling
                                basic_filebuf::sync when a get area exists
                            (27.9.1.5) | |
| No effect. | |
The type of
                                regex_constants::error_type (28.5.3) | |
| Unscoped enumeration types. | |
The values of various
                                ATOMIC_..._LOCK_FREE macros (29.4) | |
| Not supported. | |
Whether get_pointer_safety
                            returns pointer_safety::relaxed or
                                pointer_safety::preferred if the implementation has relaxed
                            pointer safety (29.4) | |
| Relaxed pointer safety. | |
The presence and meaning of
                                native_handle_type and
                                native_handle (30.2.3) | |
| Native handles are not supported. | |
The type of
                                ios_base::streamoff (D.6) | |
long long int | |
The type of
                                ios_base::streampos (D.6) | |
Typedef fpos<mbstate_t> | |