18.2.3 Enable the FPU Device
On devices with a FPU, and for applications where code may be generated
using the Floating Point Unit, the unit will be enabled. This step is only performed if the
-mfloat-abi=hard|softfp
option is in effect at the linker step, which
is the default behavior for devices which have an FPU present.