4.4.1 XC32 (Global Options)

Set up global options for all 32-bit language tools. See also “Options Page Features”.

Table 4-1. XC32 (Global Options) All Options Category
OptionDescriptionCommand Line

Stack Smashing Protector

Selects those functions protected from stack overflow.

-fstack-protector

-fstack-protector-strong

-fstack-protector-all

Override default device supportThe Do not override selection will let the MPLAB X IDE provide a list of its own DFPs that can be selected. The Compiler location will use the DFPs that ship with the compiler rather than the IDE.-mdfp
Don’t delete intermediate filesDon’t delete intermediate Files. Place them in the object directory and name them based on the source file.-save-temps=obj
Link-Time OptimizationsWhen this feature is enabled, the build will be constrained in the following ways:

- The per-file build settings will be ignored

- The build will no longer be an incremental one (full build only)

-flto
Common include dirsDirectory paths entered here will be appended to the already existing include paths of the compiler.

Relative paths are from the MPLAB X IDE project directory.

-I dir
Data TCM size in bytesEnable data Tightly Coupled Memory with the specified size. -mdtcm=n where n is the size specified by user
Instruction TCM size in bytesEnable instruction Tightly Coupled Memory with the specified size.-mitcm=n
Locate stack data in TCMLocate the stack in data Tightly Coupled Memory.-mstack-in-tcm