16.2 Function Attributes and Specifiers
The compiler keyword __attribute__ allows you to
specify special attributes of functions. This keyword is followed by an attribute
specification inside double parentheses.
You may also specify attributes with __ (double
underscore) preceding and following each keyword (e.g., __noreturn__
instead of noreturn). This allows you to use them in header files
without being concerned about a possible macro of the same name.
To specify multiple attributes, separate them by commas within the
double parentheses, for
example:
__attribute__ ((address(0x100), keep))The attribute specifier can be placed either before or after the function's return type.
Note: It is important to use function attributes consistently
throughout a project. For example, if a function is defined in file A with the an
attribute, and declared
extern in file B without the same attribute,
then a link error might result.