6.2.3 Multi-Step C Compilation
Make utilities and IDEs, such as MPLAB X IDE, allow for an incremental build of projects that contain multiple source files. When building a project, they take note of which source files have changed since the last build and use this information to speed up compilation.
For example, if compiling two source files, but only one has changed since the last build, the intermediate file corresponding to the unchanged source file need not be regenerated.
If the compiler is being invoked using a make utility, the make file will
need to be configured to use the intermediate files (.o files) and the
options used to generate the intermediate files (-c, see Options for Controlling the Kind of Output). Make utilities
typically call the compiler multiple times: once for each source file to generate an
intermediate file, and once to perform the second stage compilation.
ex1.c and add.c
listed in Single-Step C Compilation subsection
"Compiling Multiple C Files" can be compiled separately
with:xc32-gcc -mprocessor=ATSAME54P20A
-mdfp="Microchip/SAME54_DFP/3.9.244" -c ex1.c
xc32-gcc -mprocessor=ATSAME54P20A
-mdfp="Microchip/SAME54_DFP/3.9.244" -c add.c
xc32-gcc -mprocessor=ATSAME54P20A
-mdfp="Microchip/SAME54_DFP/3.9.244" -o ex1.elf ex1.o add.o