6.7.11.1 B: Specify Compiler Component Search Path Option
The -Bprefix option specifies a path where executables,
libraries, include files and compiler data files can be found.
The compiler driver runs one or more of the internal applications
xc32-cpp, xc32-as and xc32-ld. It tries
prefix as a prefix for each application it tries to
run.
For each application to be run, the compiler driver first tries adding
prefix. If the application cannot be found, the
driver searches the search paths specified by the PATH environment
variable for the application.
If prefix specifies a directory name, this path also
applies to libraries used by the linker, because the driver translates this into
-L options for the linker. This also applies to include file search
paths, because the compiler translates these options into -isystem options
for the preprocessor. In this case, the compiler appends include to the
prefix.