6.3.2 Compiling Multiple C++ Files
This section demonstrates how to compile and link multiple C and C++ files in a single step.
File 1
/* ex1.cpp */
#pragma config WDT_ENABLE = OFF // Watchdog Timer: Disabled
#pragma config BOD33_DIS = DISABLED // BOD33: Disabled
#pragma config NVMCTRL_REGION_LOCKS = 0xFFFF // NVM region locks: None
#include <xc.h>
#include <iostream>
using namespace std;
extern unsigned int add(unsigned int a, unsigned int b);
int main(void) {
int myvalue = 6;
std::cout << "original value: " << myvalue << endl;
myvalue = add(myvalue, 3);
std::cout << "new value: " << myvalue << endl;
while (1);
}File 2
/* add.cpp */
unsigned int add(unsigned int a, unsigned int b) {
return(a+b);
}Compile both files by typing the following at the
prompt:
xc32-g++ -mprocessor=ATSAME54P20A
-mdfp="Microchip/SAME54_DFP/3.9.244" -Wl,--defsym=_min_heap_size=0xF000 -o ex1.elf ex1.cpp add.cppThe command compiles the modules ex1.cpp and add.cpp. The compiled modules are linked with the compiler libraries for C++, a heap is provided, and the executable file ex1.elf is created.
Note: Use the
xc32-g++ (as opposed to the xc32-gcc driver) in order to link the
project with the C++ support libraries necessary for the C++ source file in the
project.