9.10.1 Thread Qualifier
The compiler's Thread-Local Storage (TLS) feature ensures that the compiler and libraries
create an independent instance of each __thread-qualified object in
each thread executed by the program. Thus, because they are not shared, these objects
are accessed without data corruption or unexpected behavior across multiple threads and
are known as thread-safe objects.
Thread-safe objects can be initialized when they are defined, if required. They cannot
use the persistent or address attributes, but they
can, however, be placed in a user-defined section using the section
attribute. Objects with automatic storage duration are inherently thread safe, so using
the __thread qualifier with them makes no sense, but objects with
permanent storage duration can be made thread-safe. Use of the
space(data) attribute with the __thread qualifier
is valid but has no effect; use of the space(prog) attribute and this
qualifier will result in an error.
__thread int result;
__thread __attribute__((section("my_section"))) int var = 7;If the TLS is not enabled, the __thread qualifier is ignored and any
object using it is linked and accessed like an ordinary C object.