3 Getting Started
The following resources are available to get started with the PIC32CZ CA70/MC70 MCU family, MPLAB® Harmony v3 framework, MPLAB Code Configurator (MCC), MPLAB Code Configurator Content Manager (CM), and MPLAB X IDE.
- Microchip Developer Help:
- Access the Microchip Developer Help website, which provides documentation, tutorials, and examples specific to the PIC32CZ CA70/MC70 family of devices.
- Community and Support:
- Utilize Microchip forums for any issues during the migration process. Microchip's community is very active and provides substantial support for migrating from other families.
- Example Projects:
- Review example projects from MPLAB Harmony and MPLAB X IDE example collections for the PIC32CZ CA70/MC70 family of devices.
Reference Demos:
- Getting Started Application using Harmony v3 Drivers on SAM E70 Xplained Ultra Evaluation Kit
- Getting Started Application using Harmony v3 Drivers and FreeRTOS on SAM E70 Xplained Ultra Evaluation Kit
- Getting Started Application on SAM E70 Xplained Ultra Evaluation Kit
- PIC32CZ CA70 Applications
Note: The above list provides the reference demonstrations for the SAM
E70/S70/V70/V71 devices. Because the PIC32CZ CA70/MC70 family is pin-to-pin
compatible with the SAM E70/S70/V70/V71 family of MCUs, the reference demos
on the SAM E70/S70/V70/V71 can be used as a starting point. Also, note that
the same demonstration can be easily ported to the PIC32CZ CA70 as explained
in the point 2 of the FAQs
section.
Technical Briefs:
- How to Setup MPLAB Harmony v3 Software Development Framework (DS90003232)
- Create a new MPLAB Harmony v3 project using MCC
- How to Build an Application by Adding a New PLIB, Driver, or Middleware to an Existing MPLAB Harmony v3 Project (DS90003253)
- Video - How to Set up the Tools Required to Get Started with MPLAB® Harmony v3 and MCC
Migration Guides to Help Users Get Started with MPLAB Harmony v3 Framework:
- MPLAB Harmony v3 Project Migration (DS00004495)
Application Notes:
Training Modules:
GitHub Repositories:
- https://github.com/Microchip-MPLAB-Harmony/reference_apps
- https://github.com/Microchip-MPLAB-Harmony/quick_docs
- github.com/Microchip-MPLAB-Harmony/csp_apps_pic32cz_ca70
- github.com/Microchip-MPLAB-Harmony/core_apps_pic32cz_ca70
- github.com/Microchip-MPLAB-Harmony/net_apps_pic32cz_ca70
- github.com/Microchip-MPLAB-Harmony/gfx_apps_pic32cz_ca70_mc70
MPLAB Discover References:
- PIC32CZ CA70
- PIC32CZ MC70