3.7 PIC32MZ2051W1 Python 3 Information
This section describes the Python 3 example information of the PIC32MZ2051W1. For more details, refer to the Python3_Example.chm.
The user can refer to the example code in the PIC32MZ2051W1 package example folder, which provides details on how to use the PIC32MZ2051W1.dll file with the Python language to control the PIC32MZ2051W1. For more details, refer to How to Run Python 3.6 Environment.