All the applications listed in this user’s guide use the Universal Asynchronous
Receiver/Transmitter (UART) interface on SAML21 Xplained Pro to send the status
messages, like Scanning, Advertising, Connected and the sensor data, from a remote
device. Any serial application (for example: Tera Term) can be used to interact with
SAML21 Xplained Pro.
The following table provides the UART (COM port) settings to be used to communicate with
the SAML21 Xplained Pro.
Figure 3-3. UART (COM Port)
Settings
The following are the steps to configure the serial console setup:
Open any serial application, like
Tera Term.
Connect the enumerated COM port
on Tera Term as illustrated in the following figure.
Figure 3-4. Tera Term Application
Refer to Figure 3-3 for the Tera Term serial port
setup.
Figure 3-5. Tera Term Serial Port Setup
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.