4 How to Use the Results

The results returned from the tool not only provide a side-by-side view but also highlight differences and potential impacts, which can be sorted and collected by type or severity by the tool. A design checklist can be generated and used to guide the manual inspection of the input data to ensure accuracy and correctness. The results should always be checked against the input data. If errors are found, the prompt may need to be modified or expanded, or additional data may need to be provided.