2.8 ModelInfo Object

The ModelInfo object holds additional model-specific information about a secure sub-system device that is not captured by the other cryptographic members. It has no specific members, but depends on the model of the secure sub-system device.

At this time, the ModelInfo object is defined only for the CryptoAuthentication™ ATECC608 model.