4.2.2 Analog Power Supply
These devices have a separate analog supply pin AVDD for future compatibility. In this device, the AVDD and VDD power domains are internally connected.
The following figure shows the recommendation for connecting a power supply to the AVDD pin of the device.
Important: For systems that
frequently cycle VDD or experience fast VDD transients, it is
recommended to add an additional decoupling capacitor (C3) if the power
supply slew rate exceeds the slew rate limits. Refer to the Supply Voltage section
in the Electrical Characteristics for details about power supply slew rate limits.