5.1 Application Code Update in Atmel Studio
Todo:
- Update main.c to disable the digital input buffer on all I/O pins.
- Update driver_isr.c to configure the USART TX pin as output pin during data transmission and as input pin during no data transmission period.
- Edit the main.c file:
- Disable the digital input buffer on all
I/O pins by adding in the following function before the
main()function.//Disable digital input buffer on all IO pins void io_init(void) { for (uint8_t pin=0; pin < 8; pin++) { (&PORTA.PIN0CTRL)[pin] = PORT_ISC_INPUT_DISABLE_gc; //Disable on PAx pin (&PORTB.PIN0CTRL)[pin] = PORT_ISC_INPUT_DISABLE_gc; //Disable on PBx pin (&PORTC.PIN0CTRL)[pin] = PORT_ISC_INPUT_DISABLE_gc; //Disable on PCx pin } }Info: PORT_ISC_INPUT_DISABLE_gc will set the digital input buffer disabled. Hover over it and right-click ->Goto Implementation will open the iotn817.h file and point to where it is defined. - Call the function by adding the
following code after the atmel_start_init(); line in main() function.
//Disable digital input buffer on all IO pins io_init();
- Disable the digital input buffer on all
I/O pins by adding in the following function before the
- Edit the driver_isr.c file:
- Add the following line of code at the
start of the
ISR(ADC0_RESRDY_vect)function:VPORTB.DIR |= PIN2_bm; //Configure USART TX pin PB2 as output pin - Add the following line of code after
the USART transmission is completed in the
ISR(ADC0_RESRDY_vect)function:VPORTB.DIR &= ~PIN2_bm; //Configure USART TX pin PB2 as inputInfo: This will configure the USART TX pin as an input. The reason behind is that, when the USART TX pin is configured as an output, there will be a current flow between the on-chip TX pin and the onboard EDBG pin since there are supply voltage variations between them. By configuring it as input while there is no data transmission, unnecessary current flow is avoided.
- Add the following line of code at the
start of the
- Program the device by clicking Debug → Start without Debugging on the top menu window or by using the shortcut Ctrl+Alt+F5
Info: Start
Without Debugging will build the project and program the device as long as there are no
build errors.