31.3.3.4 Output Formats
The output from an ADC conversion is given by the following equations:
Where VINP is the positive input to the ADC, RES is the conversion result, and VREF is the selected voltage reference.
The ADC has two output registers, the Sample (ADCn.SAMPLE) and Result (ADCn.RESULT) registers. The 16-bit Sample register will always be updated with the latest ADC conversion output (one sample). All accumulation modes will accumulate samples in an internal sample accumulator, configured by the Sample Accumulation Number Select (SAMPNUM) bit field in the Control F (ADCn.CTRLF) register. The sample accumulator is sufficiently wide to avoid overflow for all supported accumulation configurations. The accumulated result will automatically be transferred to the 16-bit Result register at the end of a Burst or Series mode accumulation. In single conversion modes, the Result register will be updated with the latest sample, identical to the Sample (ADCn.SAMPLE) register.
The Left Adjust (LEFTADJ) bit in the Control F (ADCn.CTRLF) register enables left shift of the output data in the modes where this is supported. If enabled, this will left shift the output from both the Result (ADCn.RESULT) and the Sample (ADCn.SAMPLE) registers.
The data format for a sample is an unsigned number, where 0x000
represents zero, and 0x3FF represents the largest number (full scale).
If the analog input is higher than the reference level of the ADC, the 10-bit ADC output
will be equal to the maximum value of 0x3FF. Likewise, if the input is
below 0V, the ADC output will be 0x000.
The following table shows the Result register output formats by mode of operation and left adjustment.
| MODE | LEFTADJ | RES[15:12] | RES[11:8] | RES[7:0] |
|---|---|---|---|---|
0 | X(1) | 0x00 | Conversion[7:0] | |
1 | 0 | 0x00 | Conversion[9:0] | |
| 1 | Conversion[9:0] << 4 | |||
2, 3 | X(1) | Accumulation[15:0] | ||
- Left adjust is not available in 8-bit mode or accumulation modes.
The following table shows the Sample register output formats by mode of operation and left adjustment.
| MODE | LEFTADJ | SAMPLE[15:12] | SAMPLE[11:8] | SAMPLE[7:0] |
|---|---|---|---|---|
0 | X | 0x00 | Conversion[7:0] | |
| Sign extension | Signed conversion[7:0] | |||
Other | 0 | 0x00 | Conversion[9:0] | |
| Sign extension | Signed conversion[9:0] | |||
| 1 | Conversion[9:0] << 4 | |||
| Signed conversion[9:0] << 4 | ||||