10.8.2 Volatile Type Qualifier
The volatile type qualifier is used to tell the compiler
that an object cannot be guaranteed to retain its value between successive accesses. This
prevents the optimizer from eliminating apparently redundant references to objects declared
volatile because it may alter the behavior of the program to do so.
Any SFR which can be modified by hardware or which drives hardware is
qualified as volatile, and any variables which may be modified by
interrupt routines should use this qualifier as well. For example:
extern volatile unsigned int INTCON1
__attribute__((__sfr__));
The code produced by the compiler to access volatile
objects may be different to that to access ordinary variables, and typically the code will
be longer and slower for volatile objects, so only use this qualifier if
it is necessary. Failure to use this qualifier when it is required, may lead to code
failure.
Another use of the volatile keyword is to prevent
variables being removed if they are not used in the C source. If a
non-volatile variable is never used, or used in a way that has no
effect on the program’s function, then it may be removed before code is generated by the
compiler.
A C statement that consists only of a volatile variable’s
name will produce code that reads the variable’s memory location and discards the result.
For example the entire statement:
PORTB;
will produce assembly code the reads PORTB, but does
nothing with this value. This is useful for some peripheral registers that require reading
to reset the state of interrupt flags. Normally such a statement is not encoded as it has
no effect.
Some variables are treated as being volatile even though
they may not be qualified in the source code. See Mixing C and Assembly Code if you have assembly
code in your project.