4.3.3 Header File Specification
Header file specifications that use directory separators do not conform to the CCI.
Example
The following example shows two conforming include directives.
#include <usb_main.h>
#include "global.h"
Differences
Header file specifications that use directory separators have been allowed
in previous versions of all compilers. Compatibility problems arose when Windows-style
separators “\” were used and the code was compiled under other host
operating systems. Under the CCI, no directory separators should be used.
Migration to the CCI
Any #include directives that use directory separators in
the header file specifications should be changed. Remove all but the header file name in
the directive. Add the directory path to the compiler’s include search path or MPLAB X IDE
equivalent. This will force the compiler to search the directories specified with this
option.
For example, the following code:
#include <inc/lcd.h>
should be changed to:
#include <lcd.h>
and the path to the inc directory added to the compiler’s
header search path in your MPLAB X IDE project properties, or on the command line as
follows:
-Ilcd