4.3.14 Bit-fields Straddling a Storage Unit Boundary
The standard indicates that implementations can determine whether bit-fields cross a storage unit boundary. In the CCI, bit-fields do not straddle a storage unit boundary; a new storage unit is allocated to the structure, and padding bits fill the gap.
Note that the size of a storage unit differs with each compiler, as this
is based on the size of the base data type (e.g., int) from which the
bit-field type is derived. On 8-bit compilers this unit is 8-bits in size; for 16-bit
compilers, it is 16 bits; and for 32-bit compilers, it is 32 bits in size.
Example
The following example shows a structure containing bit-fields being defined.
struct {
unsigned first : 6;
unsigned second :6;
} order;
Under the CCI and using MPLAB XC8, the storage allocation unit is byte
sized. The bit-field, second, is allocated a new storage unit since there
are only 2 bits remaining in the first storage unit in which first is
allocated. The size of this structure, order, is 2 bytes.
Differences
This allocation is identical with that used by all previous compilers.
Migration to the CCI
No action required.