23.21 exit
What is the status returned by the exit function if the value of the argument is other than zero, EXIT_SUCCESS, or EXIT_FAILURE? (ISO 7.10.4.3)
The value of the argument.
What is the status returned by the exit function if the value of the argument is other than zero, EXIT_SUCCESS, or EXIT_FAILURE? (ISO 7.10.4.3)
The value of the argument.
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.