5.3.7.7 How Do I Make a Function Wrapper For an Assembly Module?
The C compiler expects all C visible names to start with a leading underscore. In order to export a function to C code from assembly code, it must be globally visible. Of course, there should also be an external prototype in C so that the compiler can properly see it.
foo.s:
.text
.global _foo
_foo: retlw #0,w0
main.c:
extern int foo(void);
For details on using C code with an assembly module, see the following section of this user’s guide: