10.6.4 Special Pointer Targets
Pointers and integers are not interchangeable. Assigning an integer value to a pointer will generate a warning to this effect. For example:
const char * cp = 0x123; // the compiler will flag this as bad
code
There is no information in the integer, 0x123, relating to the type, size
or memory location of the destination. Avoid assigning an integer (whether it be a constant
or variable) to a pointer at all times. Addresses assigned to pointers should be derived
from the address operator "&" that C provides.
In instances where you need to have a pointer reference a seemingly
arbitrary address or address range, consider defining an object or label at the desired
location. If the object is defined in assembly code, use a C declaration (using the
extern keyword) to create a C object which links in with the external
object and whose address can be taken.
Take care when comparing (subtracting) pointers. For example:
if(cp1 == cp2)
; take appropriate action
The ANSI C standard only allows pointer comparisons when the two pointer targets are the same object. The address may extend to one element past the end of an array.
Comparisons of pointers to integer constants are even more risky, for example:
if(cp1 == 0x246)
; take appropriate action
A NULL pointer is the one instance where a constant value
can be safely assigned to a pointer. A NULL pointer is numerically equal
to 0 (zero), but since they do not guarantee to point to any valid object and should not be
dereferenced, this is a special case imposed by the ANSI C standard. Comparisons with the
macro NULL are also allowed.