7.2.1 Register Definition Files
The processor header files described in 7.2 Device Header Files name all SFRs for each
part, but they do not define the addresses of the SFRs. A separate set of device-specific
linker script files, one per part, is distributed in the
support/family/gld directory. These linker script
files define the SFR addresses. To use one of these files, specify the linker command-line
option:
-T pdevice.gld
where device corresponds to an
abbreviated device number.
For example, assuming that there is a file named app504.c
that contains an application for the dsPIC33EP512MC504 part, then it may be compiled and
linked using the following command line:
xc-dsc-gcc -mcpu=33EP512MC504 -o
app504.out -T p33EP512MC504.gld app504.c
The -o command-line option names the output executable
file, and the -T option gives the linker script name for the
dsPIC33EP512MC504 part. If p33EP512MC504.gld is not found in the current
directory, the linker searches in its known library paths. The default search path includes
all locations of preinstalled libraries and linker scripts.
It is unlikely that you will need to customize a linker script but if you do, you should copy the appropriate linker script file (supplied with the compiler) into your project directory before any project-specific modifications are made.