11.3 Variables in Program Space
The DSC core families of processors contain hardware support for accessing data from within program Flash using a hardware feature that is commonly called Program Space Visibility (PSV). More detail about how PSV works can be found in device data sheets or Family Reference Manuals (see sections 11.3.1 Allocation and Access of Program Memory Objects and 15.7.2 PSV Usage with Interrupt Service Routines).
The architecture allows the mapping of one 32K page of Flash into the
upper 32K of the data address space via the Special Function Register (SFR) PSVPAG or
DSRPAG. By default, the compiler only supports direct access to one single PSV page,
referred to as the auto_psv space. In this model, DSC data pointers can be used. However, this can make it
difficult to manage large amounts of constant data stored in Flash on larger devices.
When the option -mconst-in-code is enabled,
const-qualified variables that are not auto are placed
in program memory. Any auto variables qualified const are
placed on the stack along with other auto variables.
Any const-qualified (auto or
non-auto) variable will always be read-only and any attempt to write to
these in your source code will result in an error being issued by the compiler.
A const object is usually defined with initial values, as
the program cannot write to these objects at runtime. However this is not a requirement. An
uninitialized const object is allocated space along with other
uninitialized RAM variables, but is still read-only. Here are examples of
const object definitions.
const char IOtype = ’A’; // initialized const object
const char buffer[10]; // I reserve memory in RAM
See the 17 Mixing C and Assembly Code section for the equivalent assembly symbols that are used to represent
const-qualified variables in program memory.