5.6 Project Setup
To set up an MPLAB X IDE project for the first time, use the built-in Project Wizard (). In this wizard, you will be able to select a language toolsuite that uses the XC-DSC language tools. For more on the wizard and MPLAB X IDE projects, see MPLAB X IDE documentation.
Once you have a project set up, you may then set up properties of the tools in MPLAB X IDE (see figure below).
- From the MPLAB X IDE menu bar, select to open a window to set/check project build options.
- Under Conf:[
default], select a tool from the tool collection to set up.Figure 5-3. Project Properties Window