2.5.3.3.2 Transparent Control Point Characteristic Behavior

While the Transparent Control Point is used by a Client to control certain behaviors of the Server. The procedures are triggered by writing a Characteristic Value that includes an opcode specifying the operation and the Server will notify the result of the operations.

While the Transparent Control Point is used by a Server to control certain behaviors of the Client. The procedures are triggered by notifying a Characteristic Value that includes an opcode specifying the operation and Client will write the result of the operations.

For each procedure is described in the next section.