GATTS_AddService
C
uint16_t GATTS_AddService(GATTS_Service_T *p_service, uint8_t numAttributes);
Description
This API registers service to GATT server.
Note
Note that the start handle of the registering service should be greater than GATTS_APP_SVC_START_HDL.
Parameters
Parameter | Description |
---|---|
[in] p_service | Pointer to the registering service information. |
[in] numAttributes | Number of the attributes in the registering service. |
Return values
Return value | Description |
---|---|
MBA_RES_SUCCESS | Successfully registering the service. |
MBA_RES_FAIL | Fail to register the service. The assigned attribute handles in the service conflict or the start handle of the service is smaller than GATTS_APP_SVC_START_HDL. |