BLE_HOGPS_SetKeyboardInputReport
C
uint16_t BLE_HOGPS_SetKeyboardInputReport(uint8_t *p_keyCodeArray);
Description
Set HID keyboard input report.
Parameters
Parameter | Description |
---|---|
[in] p_keyCodeArray | 8 bytes of key codes array. From byte 0 to byte 7: |Modifier Keys|Reserved|Keycode 1|Keycode 2|Keycode 3|Keycode 4|Keycode 5|Keycode 6|. |
Return values
Return value | Description |
---|---|
MBA_RES_SUCCESS | Successfully set the input report. |
MBA_RES_INVALID_PARA | Invalid parameters. |