BLE_DTM_TransmitterTestParams_T

C

typedef struct BLE_DTM_TransmitterTestParams_T
{
    uint8_t                 txChannel;
    uint8_t                 testDataLen;
    uint8_t                 packetPayload;
    uint8_t                 phy;
    int8_t                  transmitPowerLevel;
} BLE_DTM_TransmitterTestParams_T;

Description

Transmitter test parameters.

Field Documentation

FieldDescription
txChannelThe RF channel which is used by the transmitter. Channel= (F – 2402) / 2 (Frequency Range : 2402 MHz to 2480 MHz) See Receiver or transmitter channel.
testDataLenThe length of the payload of the test reference packets.
packetPayloadThe contents of the payload of the test reference packets. See Transmitter payload type.
phyThe PHY which is used by the transmitter. See Transmitter PHY type.
transmitPowerLevelThe transmit power level which is used by the transmitter. Range: -127 to +20. (Units: dBm) Set to 0x7E to use the minimum transmit power level. Set to 0x7F to use the maximum transmit power level. If the parameter is set to a value other than 0x7E or 0x7F, then ble stack makes the requested change or makes closest change that it is capable of doing.