BLE_HOGPS_EventId_T
C
typedef enum BLE_HOGPS_EventId_T
{
BLE_HOGPS_EVT_BOOT_MODE_ENTER_IND = 0x00U,
BLE_HOGPS_EVT_REPORT_MODE_ENTER_IND,
BLE_HOGPS_EVT_HOST_SUSPEND_ENTER_IND,
BLE_HOGPS_EVT_HOST_SUSPEND_EXIT_IND,
BLE_HOGPS_EVT_INPUT_REPORT_WRITE_IND,
BLE_HOGPS_EVT_OUTPUT_REPORT_WRITE_IND,
BLE_HOGPS_EVT_FEATURE_REPORT_WRITE_IND,
BLE_HOGPS_EVT_BOOT_KB_INPUT_REPORT_WRITE_IND,
BLE_HOGPS_EVT_BOOT_KB_OUTPUT_REPORT_WRITE_IND,
BLE_HOGPS_EVT_BOOT_M_INPUT_REPORT_WRITE_IND,
BLE_HOGPS_EVT_END
} BLE_HOGPS_EventId_T;
Description
Enumeration for BLE HID over GATT Profile (HOGP) service callback events.
Enumerator | Description |
---|---|
BLE_HOGPS_EVT_BOOT_MODE_ENTER_IND | Event indicating the device has entered HID Boot Mode. See BLE_HOGPS_EvtBootModeEnter_T for event details. |
BLE_HOGPS_EVT_REPORT_MODE_ENTER_IND | Event indicating the device has entered HID Report Mode. See BLE_HOGPS_EvtReportModeEnter_T for event details. |
BLE_HOGPS_EVT_HOST_SUSPEND_ENTER_IND | Event indicating the HID host is entering suspend mode. See BLE_HOGPS_EvtHostSuspendEnter_T for event details. |
BLE_HOGPS_EVT_HOST_SUSPEND_EXIT_IND | Event indicating the HID host is exiting suspend mode. See BLE_HOGPS_EvtHostSuspendExit_T for event details. |
BLE_HOGPS_EVT_INPUT_REPORT_WRITE_IND | Event indicating an HID Input Report has been written. See BLE_HOGPS_EvtReportWrite_T for event details. |
BLE_HOGPS_EVT_OUTPUT_REPORT_WRITE_IND | Event indicating an HID Output Report has been written. See BLE_HOGPS_EvtReportWrite_T for event details. |
BLE_HOGPS_EVT_FEATURE_REPORT_WRITE_IND | Event indicating an HID Feature Report has been written. See BLE_HOGPS_EvtReportWrite_T for event details. |
BLE_HOGPS_EVT_BOOT_KB_INPUT_REPORT_WRITE_IND | Event indicating a Boot Keyboard Input Report has been written. See BLE_HOGPS_EvtBootReportWrite_T for event details. |
BLE_HOGPS_EVT_BOOT_KB_OUTPUT_REPORT_WRITE_IND | Event indicating a Boot Keyboard Output Report has been written. See BLE_HOGPS_EvtBootReportWrite_T for event details. |
BLE_HOGPS_EVT_BOOT_M_INPUT_REPORT_WRITE_IND | Event indicating a Boot Mouse Input Report has been written. See BLE_HOGPS_EvtBootReportWrite_T for event details. |
BLE_HOGPS_EVT_END | Sentinel value indicating the end of the event enumeration. |