MW_DFU_FwImageStart

C

uint16_t MW_DFU_FwImageStart(void);

Description

Starts or restarts the firmware image update procedure.

Note

Calling this API resets the state machine and parameters of the DFU module.

Return values

Return valueDescription
MBA_RES_SUCCESSFirmware image update procedure started or restarted successfully.
MBA_RES_BAD_STATEThe API cannot be executed in the current state of the DFU process.