BLE_TRCBPS_SendVendorCommand
C
uint16_t BLE_TRCBPS_SendVendorCommand(uint16_t connHandle, uint8_t cmdId, uint16_t len, uint8_t *p_payload);Description
Send a vendor-specific command through the BLE TRCBP Control pipe.
Parameters
| Parameter | Description |
|---|---|
| [in] connHandle | Connection handle. |
| [in] cmdId | Vendor command Opcode (see TRCBPS vendor opcodes). |
| [in] len | Length of the vendor command. |
| [in] p_payload | Pointer to the command payload. |
Return values
| Return value | Description |
|---|---|
| MBA_RES_SUCCESS | Successfully sent the vendor command. |
| MBA_RES_OOM | Internal memory allocation failure. |
| MBA_RES_INVALID_PARA | Invalid L2CAP link or data length exceeds max MTU. |
| MBA_RES_BAD_STATE | Connection not established. |