BT_SYS_TraceEnable
C
void BT_SYS_TraceEnable(BT_SYS_TraceFmt_T fmt, uint32_t traceMask, BT_SYS_TraceEventCb_T traceCb);Description
Enable Bluetooth system trace message indications.
Parameters
| Parameter | Description |
|---|---|
| [in] fmt | The format of the trace messages. See Trace format for possible values. |
| [in] traceMask | A bitmask that specifies which trace messages to enable. See Trace mask for details. BT system trace mask. |
| [in] traceCb | The callback function that will be invoked for trace events. See @ref BT_SYS_TraceEventCb_T. See BT_SYS_TraceEventCb_T. |