BLE_GAP_SetPeriAdvEnable
C
uint16_t BLE_GAP_SetPeriAdvEnable(uint8_t enable, uint8_t advHandle);Description
Enables or disables periodic advertising for a specified advertising set.
Note
If the advertising set is not currently enabled (see BLE_GAP_SetExtAdvEnable), periodic advertising will not start until the advertising set is enabled. Periodic advertising continues until this API is called with 'enable' set to false. This API is part of the extended advertising feature and is disallowed if any legacy advertising feature API has been used previously. See Categories of advertising APIs and events for details on advertising APIs. Initialization with BLE_GAP_AdvInit, BLE_GAP_ExtAdvInit, and BLE_GAP_PeriodicAdvInit is required before using this API.
Parameters
| Parameter | Description |
|---|---|
| [in] enable | Set Options for enabling periodic advertising to enable periodic advertising; otherwise, set it to 0. |
| [in] advHandle | Advertising set identifier to enable or disable periodic advertising for. |
Return values
| Return value | Description |
|---|---|
| MBA_RES_SUCCESS | Successfully enables or disables the periodic advertising. |
| MBA_RES_OOM | Internal memory allocation failure occurred. |
| MBA_RES_INVALID_PARA | The parameters provided are invalid. |
| MBA_RES_COMMAND_DISALLOWED | Command disallowed due to a conflicting operation or state. |
| MBA_RES_UNKNOWN_ADV_ID | Unknown advertising identifier. |