BT_SYS_Cfg_T
PIC32CX-BZ2
C
typedef struct BT_SYS_Cfg_T
{
int8_t antennaGain;
unsigned int addrValid:1;
unsigned int rssiOffsetValid:1;
uint8_t devAddr[BT_SYS_DEV_ADDR_LEN];
int8_t rssiOffset;
} BT_SYS_Cfg_T;Description
Structure for Bluetooth system configuration.
Field Documentation
| Field | Description |
|---|---|
| antennaGain | Antenna gain in dB. |
| addrValid | Flag indicating if the device address is valid (1) or not (0). |
| rssiOffsetValid | Flag indicating if the RSSI offset is valid (1) or not (0). |
| devAddr | Bluetooth device address in hex format. |
| rssiOffset | Offset to be applied to the RSSI value. |
PIC32CX-BZ3 and PIC32CX-BZ6
C
typedef struct BT_SYS_Cfg_T
{
int8_t antennaGain;
unsigned int addrValid:1;
unsigned int rssiOffsetValid:1;
unsigned int adcTimingValid:1;
uint8_t devAddr[BT_SYS_DEV_ADDR_LEN];
int8_t rssiOffset;
uint8_t adcTiming08;
uint8_t adcTiming51;
} BT_SYS_Cfg_T;Description
Structure for Bluetooth system configuration.
Field Documentation
| Field | Description |
|---|---|
| antennaGain | Antenna gain in dB. |
| addrValid | Flag indicating if the device address is valid (1) or not (0). |
| rssiOffsetValid | Flag indicating if the RSSI offset is valid (1) or not (0). |
| adcTimingValid | Flag indicating if the RSSI offset is valid (1) or not (0). |
| devAddr | Bluetooth device address in hex format. |
| rssiOffset | Offset to be applied to the RSSI value. |
| adcTiming08 | ADC timing value for RF register 08, used for configuring ADC operation. |
| adcTiming51 | ADC timing value for RF register 51, used for configuring ADC operation. |