BT_SYS_LogEvent_T
C
typedef struct BT_SYS_LogEvent_T
{
uint16_t logType;
uint16_t logId;
uint16_t paramsLength;
uint16_t payloadLength;
uint8_t *p_logPayload;
uint8_t *p_returnParams;
} BT_SYS_LogEvent_T;Description
Structure for a Bluetooth system log event.
Field Documentation
| Field | Description |
|---|---|
| logType | Type of the log event, indicating the category or source of the event. |
| logId | Unique identifier for the log event. When logType corresponds to BT_SYS_LOG_TYPE_HCI_ACL_TX or BT_SYS_LOG_TYPE_HCI_ACL_RX data, this represents the connection handle. |
| paramsLength | Length of the additional parameters associated with the log event. A value of 0 indicates that there are no additional parameters. |
| payloadLength | Length of the payload data for the log event. A value of 0 indicates that there is no payload. |
| p_logPayload | Pointer to the payload data. A NULL pointer indicates that there is no payload. |
| p_returnParams | Pointer to the additional parameters. A NULL pointer indicates that there are no additional parameters. |