BLE_HOGPS_SetBootMouseInputReport
C
uint16_t BLE_HOGPS_SetBootMouseInputReport(uint8_t buttons, int8_t xAxis, int8_t yAxis);Description
Sets the HID boot mode mouse input report.
Note
This function prepares the input report for a mouse in HID boot mode with the current state of mouse buttons and position.
Parameters
| Parameter | Description |
|---|---|
| [in] buttons | Bitmask representing the state of the mouse buttons: - Bit 0: Left button - Bit 1: Right button - Bit 2: Middle button |
| [in] xAxis | The displacement of the mouse along the X-axis since the last report, in units. |
| [in] yAxis | The displacement of the mouse along the Y-axis since the last report, in units. |
Return values
| Return value | Description |
|---|---|
| MBA_RES_SUCCESS | The input report was successfully set. |
| MBA_RES_INVALID_PARA | The parameters provided are invalid. |