BLE_HOGPS_Init
C
uint16_t BLE_HOGPS_Init(void);Description
Initializes the BLE HID over GATT profile server role.
Return values
| Return value | Description |
|---|---|
| MBA_RES_SUCCESS | The initialization was successful. |
| MBA_RES_FAIL | The initialization failed. |
uint16_t BLE_HOGPS_Init(void);Initializes the BLE HID over GATT profile server role.
| Return value | Description |
|---|---|
| MBA_RES_SUCCESS | The initialization was successful. |
| MBA_RES_FAIL | The initialization failed. |