5.3 Programming the PolarFire Device using FlashPro Express
(Ask a Question)This section describes how to program the PolarFire Video kit, with the .job
file, using FlashPro Express. The .job file
mpf_an4576_v20xxpx_jb to test on PolarFire Video kit is provided in
the Test Setup Prerequisites section.
To program the PolarFire device, perform the following steps:
- On the host PC, start the FlashPro Express software from its installation directory.
- To create a new job project on the Project menu, click New or New Job Project from FlashPro Express Job .
- In the New Job Project from FlashPro Express Job dialog box, perform the following steps:
- Programming job file: Click Browse, navigate to the location where the
.jobfile is located and select the file. The default location is <$designfiles download directory>\mpf_an4576_v20xxpx_jb\mpf_an4576_v20xxpx_jb.job. - FlashPro Express job project location: Click Browse and navigate to the location where you want to save the project.
- Programming job file: Click Browse, navigate to the location where the
- Click OK. The required programming file is selected and ready to be programmed in the device. The FlashPro Express window appears.
- Verify that a programmer number appears in the Programmer box. If it does not, confirm the board connections and click Refresh/Rescan Programmers.
- To program the device, click RUN. When the device is programmed successfully, a RUN PASSED status is displayed.
- To close FlashPro Express, click .
The PolarFire device and SPI Flash are programmed.
Power cycle the board using the SW4 switch. After power cycling, the full HD DisplayPort monitor displays the camera feed.