5 Appendix: Running the Tcl Script
(Ask a Question)Tcl scripts are provided in www.microchip.com/en-us/application-notes/an4576.
To run Tcl, perform the following steps:
- Launch the Libero software.
- From the menu bar, click .
- In the downloaded directory
mpf_an4576_v20xxpx_df, locate and select thescript.tclfile. - To execute the selected Tcl script, click Run.
After successful execution of the Tcl script, the Libero project is created within the top directory of mpf_an4576_v20xxpx_df. You can verify the process by reviewing the log file, see mpf_an4576_v20xxpx_df_log.
For more details about the folder structure and details of the Tcl scripts and commands, see TCL_Scripts_readme.txt file and the Tcl Commands Reference Guide. Contact Technical Support for any queries about running the Tcl script.