23.3.4.4.2 Frequency Waveform Generation (FRQ)
In Frequency Generation mode, the TCEn.CMP0 register controls the period time (T), instead of the Period (TCEn.PER) register. The corresponding waveform generator output is toggled on each compare match between the TCEn.CNT and TCEn.CMPn registers.
The following equation defines the waveform frequency (fFRQ):
where N represents the prescaler divider used (see the CLKSEL bit field in the TCEn.CTRLA register), and fCLK_PER is the peripheral clock frequency.
The maximum frequency of the waveform generated is half of the
peripheral clock frequency (fCLK_PER/2) when TCEn.CMP0 is written to
0x0000, and no prescaling is used (N = 1, CLKSEL =
0x0 in TCEn.CTRLA).
Use the TCEn.CMP1 and TCEn.CMP2 registers to get additional waveform outputs WOn. The waveforms WOn can either be identical or offset to WO0. The offset can be influenced by TCEn.CMPn, TCEn.CNT and the count direction. Use the equations shown in the table below to calculate the offset in seconds (Toffset). The equations are only valid when CMPn < CMP0.
| Equation | Count Direction | CMPn vs. CNT State | Offset |
|---|---|---|---|
| UP | CMPn ≥ CNT | WOn leading WO0 | |
| DOWN | CMP0 ≤ CNT | WOn trailing WO0 | |
| CMP0 > CNT and CMPn > CNT | WOn trailing WO0 | ||
| UP | CMPn < CNT | WOn trailing WO0 | |
| DOWN | CMPn ≤ CNT | WOn leading WO0 |
The figure below shows the leading and trailing offset for WOn, where both equations can be used. The correct equation is determined by count direction and the state of CMPn vs. CNT when the timer is enabled or the CMPn is changed.
The figure below shows how the waveform can be inverted by changing the CMPn during run-time.