4 Installing the Library
To install the MCC AVR® MCU Motor Control Library:
Content Manager Wizard
- Create a new MPLAB® X project with one of the supported devices.
- Open the MCC.
- Select MCC Melody from the Content Manager Wizard start page.
- Once you see the MCC Content Manager Wizard page with required and optional content boxes, check the box located next to the AVR® MCU Motor Control Library. It can be found on this page by going to Optional Content > Libraries .
- Once the box there is checked, click Finish to start the library download.
Content Manager
- Open the MCC.
- Select Content Manager from within the Device Resources section.
- Navigate to Libraries > AVR® MCU Motor Control Library and select the desired version.
- Click Apply in the top right of the Content Manager Window.