7.2 Client Mode Reception (10-Bit Addressing)
- Host device issues a Start condition. Once the Start is detected, the client hardware sets the Start Condition Interrupt Flag (SCIF).
- Host transmits the 10-bit high address byte with R/W cleared.
- The received address is compared to
the values in the I2CxADR registers.
If the client is configured in 10-bit Addressing mode (no masking), the received high address byte is compared to the values in the I2CADR1 and I2CADR3 registers. In 10-bit Addressing mode with masking, the received address is masked with the value of I2CxADR3, and then compared to the value of I2CxADR1. If a match occurs, the R/W bit information (bit ‘
0’ of the matching address) is transferred to the Read Information (R) bit of the I2CxSTAT0 register, the Data (D) bit of the I2CxSTAT0 register is cleared, and the Address Interrupt Flag (ADRIF) bit is set. If ABD is cleared, the matching address is copied into the I2CxADB1 register. If ABD is set, the matching address is copied into the receive buffer, I2CxRXB, setting the Receive Buffer Full (RXBF) and I2C Receive Interrupt Flag (I2CxRXIF) bits. I2CRXIF is a read-only bit, and must be cleared by setting the Clear Buffer (CLRBF) bit or reading I2CxRXB.If there is not an address match, the module goes idle.
- When ADRIF is set, if the Address Interrupt and Hold Enable (ADRIE) bit is set and the Clock Stretching Disable (CSD) bit is cleared, the client hardware sets the Client Clock Stretching (CSTR) bit and the generic I2CxIF Flag bit. This allows time for the client to read either I2CxADB1 or I2CxRXB and selectively ACK/NACK based on the received address. When the client has finished processing the address, the software clears CSTR and ADRIF, which releases the clock and clears the I2CxIF bit.
- Host transmits the 9th clock pulse, and the client hardware transfers the value of the ACKDT bit onto the SDA line. If there are pending errors, such as a receive overflow, the client hardware automatically generates a NACK condition and the module goes idle.
- The host transmits the lower address
byte.
If the client is configured in 10-bit Addressing mode (no masking), the received low address byte is compared to the values in the I2CxADR0 and I2CxADR2 registers. In 10-bit Addressing mode with masking, the received address is masked with the value of I2CxADR1, and then compared to the value of I2CxADR0. If a match occurs, the Client Mode Active (SMA) bit is set, the R/W bit information is transferred to the R bit of the I2CxSTAT0 register, the D bit of the I2CxSTAT0 register is cleared, and the ADRIF bit is set. If ABD is cleared, the matching address is copied into the I2CxADB0 register. If ABD is set, the matching address is copied into the receive buffer, I2CxRXB, setting the RXBF and I2CxRXIF bits. I2CxRXIF is a read-only bit, and must be cleared by setting the Clear Buffer (CLRBF) bit or reading I2CxRXB.
- When ADRIF is set, if the ADRIE bit is set and the CSD bit is cleared, the client hardware sets the CSTR bit and the generic I2CxIF Flag bit. This allows time for the client to read either I2CxADB0 or I2CxRXB and selectively ACK/NACK based on the received address. When the client has finished processing the address, the software clears CSTR and ADRIF, which releases the clock and clears the I2CxIF bit.
- The host transmits the 9th clock pulse, and the client hardware transfers the value of the ACKDT bit onto the SDA line. If there are pending errors, such as a receive overflow, the client hardware automatically generates a NACK condition and the module goes idle.
- After the 9th falling edge of the clock, the Acknowledge Status Time Interrupt and Hold (ACKTIF) bit is set. If the Acknowledge Time Interrupt and Hold Enable (ACKTIE) bit is set, the client hardware sets the CSTR and I2CxIF bits. When the client is ready, the software clears the CSTR and ACKTIF bits, which releases SCL and clears I2CxIF.
- If the client transmits a NACK, the
host hardware generates a Stop condition. The Stop Condition Interrupt Flag (PCIF)
is set when the Stop condition is detected, and the client goes idle.
If the client issued an ACK, the host transmits the first 7 bits of the 8-bit data byte.
- If previous data are still in the
I2CxRXB register (RXBF =
1and I2CxRXIF =1) when the first seven bits of the new byte are received into the Shift register, the CSTR bit is set, and the clock is stretched after the 7th falling edge of SCL. This allows the client software to read I2CxRXB, which clears the RXBF and I2CxRXIF bits, and prevents a receive buffer overflow. Once the RXBF bit is cleared, the software releases SCL by clearing CSTR. - Host hardware transmits the 8th bit
of the current data byte into the client’s receive Shift register, then the client
hardware transfers the complete byte into I2CxRXB, sets the I2CxRXIF, the Data Write
Interrupt Flag (WRIF), the Data (D), and the RXBF bits. I2CxCNT is decremented by
one. If the Data Write Interrupt and Hold is enabled (WRIE =
1), the hardware sets CSTR, allowing time for the client software to read I2CxRXB and decide the state of the ACKDT bit before clearing CSTR. - Host transmits the 9th clock pulse.
If there are pending errors, such as a receive overflow, the client hardware
automatically generates a NACK condition, NACKIF is set, and the module goes
idle.
If I2CxCNT is not ‘
0’, the hardware transmits the value of the ACKDT bit as the ACK value to the host. It is up to the user to configure the ACKDT bit appropriately. In most cases, the ACKDT bit should be cleared, so that the host receives an ACK (logic low level on SDA during the 9th SCL pulse).If I2CxCNT is ‘
0’, the hardware transmits the value of the Acknowledge End of Count (ACKCNT) bit as the ACK value to the client. It is up to the user to properly define the ACKCNT bit. In most cases, this bit should be set, indicating a NACK condition. When the host hardware detects the NACK on the bus, the host hardware will also generate a Stop condition. If the ACKCNT bit is cleared, an ACK will be issued, and the host hardware will not automatically generate the Stop condition. - Upon the falling edge of the 9th
clock pulse, the ACKTIF bit is set, and if ACKTIE is set, the generic I2CxIF bit is
also set. If CSD = ‘
0’, the client hardware sets CSTR. This allows time for the client to read the data from I2CxRXB. Once complete, the client software clears CSTR to release the clock, and clears ACKTIF to continue communication. - Go to step 10 and continue until
I2CCNT = ‘
0’, or until the host issues a Stop condition.