5.4 Terminal Window Setting
This application uses the terminal window of the PC to print various messages and status. The device communicates with the PC (terminal window) via EDBG. The following figure shows the serial port setting to be configured at the terminal window. Here Tera Term is used as the terminal window. The user can also use the "Terminal for Atmel Studio" available as an extension in Atmel Studio